cancel
Showing results for 
Search instead for 
Did you mean: 

Can't load code on STEVAL-IDB011V1 by Keil

ELevy.1873
Associate II

Hello.

I'm using STEVAL-IDB011V1. From the BlueNRG-LP Navigator, I can load the examples on the board. But when I'm using the Keil, it says "SWD/JTAG Communication Failure".

On the options for target in the tab "Device" the device is BlueNRG-355, and the Software Pack is "Keil.STBlueNRG-LP_DFP.2.0.0". In the tab "Debug" it uses "CMSIS-DAP Debugger".

My friend has no problems with that, and we didn't find any differences between our settings.

I also updated the Keil version, and it didn't help.

Thanks.

3 REPLIES 3
Winfred LU
ST Employee

Could you please try to erase the BlueNRG-355's flash before to load code in Keil?

ELevy.1873
Associate II

No. Even when I try to erase it, it writes the same error message.

ELevy.1873
Associate II

Solved!

I checked the board very carefully and saw that jumper JP5 was broken, so I replaced it with another that I had spare, and now I can burn through the Keil.

Thanks.