2019-08-29 7:25 AM
Hello,
While booting BlueNRG2, I was in need to externally pullup the UART TX output pin for proper operation.
The (post) boot initialization examples does not pullup the pin:
/* Configure GPIO_Pin_8 and GPIO_Pin_11 as UART_TXD and UART_RXD*/
GPIO_InitStructure.GPIO_Pin = SDK_EVAL_UART_TX_PIN;
GPIO_InitStructure.GPIO_Mode = SDK_EVAL_UART_TX_MODE;
GPIO_InitStructure.GPIO_Pull = DISABLE;
Is there any reason ?
Thanks in advance.
Remy.
2019-09-01 11:49 PM
Hi Remy,
The external pull-up is not required.
Please refer to schematic of STEVAL-IDB008v2
No external pull-up is added to BlueNRG-2 DIO8.
https://www.st.com/resource/en/schematic_pack/steval-idb008v2_schematic.pdf
Best Regards,
Winfred
2019-09-05 1:44 AM
Thanks Winfred,
I had the problem on a private design and BNRG-232. I switched to -248 and added pullups on my adaptor board.
I have not checked the IDB008v2 but isn't the BNRG uart connected to the internal stlink-acting chip ?
Anyway, I'll try to remove the pullups and will post the result.
Thanks for your time.
Remy.