Hello, I do confirm BlueNRG-LP (now rebranded STM32WB07) is certified at SIG level.I would recommend having a look at our dedicated wiki certification web page.Certification guideline for STM32WB0, STM32WB and STM32WBA - stm32mcu RegardsLaurent
Hello, STM32WB05N is delivered flash free and you should flash the binary inside it.You are right at the end, this will be a DTM (in the new WB0 ecosystem, DTM is called transparent mode). Please register to STM32WB0 webinar scheduled this week.This ...
Hello Oliver,STM32WB05 is rebranding of BlueNRG-LPS.This are exacting same devices, meaning the FW you have developed for BlueNRG-LPS will run on your STM32WB05.STM32WB0x series comes with a different ecosystem (SDK and tools) versus BlueNRG, here is...
Yes I see.My request is maybe to rebuild FW with DIO7 as IRQ and modify your PCB as a test.DIO7 is the default IRQ used in our example.This is to see if this is related to DIO14 and any specifc thing around it. Laurent
Hi, No more idea on my side.May be could you confirm using DIO7 as IRQ as our default example, you can see IRQ rising up (you can add wire to modify your PCB)? Laurent