BlueNRG-345 custom board repeatedly resets due to Hardware_Code = 0x01
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-20 4:14 AM
I am working on a custom board with a BlueNRG-345 microcontroller, with the BlueNRG-LP Development kit 1.2.0 and using WiSE Studio as the development environment. I have taken the BLE Beacon project for the STEVAL-IDB011V1 and converted it to run on the BlueNRG-345 as described in section 6.2 of the Development Kit User Manual. The custom board is based on the reference design but it does not have an LSE so I have replaced the CONFIG_HW_LS_XTAL defined symbol with CONFIG_HS_LS_RO. I have commented out the call to HAL_PWR_MNGR_Request() so that I can run it under the debugger.
The project runs happily on an STEVAL-IDB011V1 but when I run it on the custom board it goes into a tight reset loop. The reason it is resetting is that the user code function hci_hardware_error_event() is being called with Hardware_Code = 0x01 and hence it calls NVIC_SystemReset(). If I change the code so that it only resets when Hardware_Code == 0x03, then the beacon functionality does work, at least for a while.
I have a separate project with the target application code and pins properly configured to match the custom hardware. This still suffers from the above problem but otherwise works fine. In this project I have avoided getting Hardware_Code = 0x01 by commenting out the calls to HAL_VTIMER_Tick() and BLE_STACK_Tick(). This appears not to stop the BLE Beacon function from working, which is fine so far as that is the only BLE function I need but it would be a problem if other BLE functions were needed in the future.
The bluenrg_lp_events.h files says that "Hardware_Code Error code 0x01 and 0x02 are errors generally caused by hardware issue on the PCB; another possible cause is a slow crystal startup." What hardware issues might be causing this or what might I have done wrong in the software?
- Labels:
-
Low Power RF Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-30 5:51 AM
Hello,
This could be related to Xtal selected for example.
Feel free to share with me your schematics (at least BlueNRg part) and Xtal full reference.
Quick tests could be
- Use LSI
If you are using a 32kHz xtal and problem is related to this, you can quickly built your application with CONFIG_HW_LS_RO pre processing option for using LSI
If this solves the problem, it means problem is related to 32kHz LSE
- Increase HSE start up time
If problem is related to HSE start up tie you can do a test pushing this value to maximum.
#define HS_STARTUP_TIME 320 // 780 us is the default setup and you can try chnage from 320 to 778 (1900 us). It will just impact a bit power consumption.
.If this solve the problem, it means problem is related to 32MHz HSE
Regards
Laurent
Regards
Laurent
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-05 2:53 AM
Hi Laurent
Thanks for responding.
- Use LSI
The board does not have an LSE so I am already using LSI by building with CONFIG_HW_LS_RO. (There is a typo in my original post.)
- Increase HSE start up time
I think I tried this before but I have tried it again anyway and it made no difference. I am still seeing hci_hardware_error_event() being called with Hardware_Code = 0x01 causing a reset loop.
This is the BlueNRG-345 part of the schematic. Hopefully this is clear enough for you to read.
The HSE, Y2, is an ECS-320-8-37CKM-TR.
Regards
Rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-05 3:35 AM
Hi Rob,
I see some problem here.
C24 should not be a cap but a 10uH coil.
Also recommended value for C32 is 220nF.
Regards
Laurent
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-05 3:41 AM
Hi Laurent
Thanks for speedy response. I've passed this information on to our hardware engineer and hopefully this will solve our problem.
Kind regards
Rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-25 3:23 AM
Hi Laurent
It turns out that our hardware guys had spotted the C24 cap/coil error already as without this change the board would not work at all. They have now changed cap C32 to 220nF and this cures the problem I was having with the firmware going into a reset loop.
Thanks very much for your help with this issue.
Kind regards
Rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-21 4:01 AM - edited ‎2024-02-22 2:53 AM
I assume mute option is ok when i solved problem?