2020-05-31 10:31 AM
While using this BlueNRG-2 sample flash code when we change our data storage address to 0x10042380 it works but only when I made that ble board boot pin ground and then high sort of reset ,then it starts working and if I change that address to 0x10070000 or 0x01050000 then it is not showing anything on Hercules then I reset again that boot pin still it is not working. Are we doing any mistake in choosing that flash address or the code dumping is not happening after changing that flash address. We want to use some flash addresses to save our valuable data in our application and for this we want some empty flash addressess.