2022-03-13 5:29 AM
Hi, I have B-U585I-IOT02A board. I'd like to log data to an uSD card. Is it possible to connect external SD Card reader along with FATFS ? If so, which protocol to use SPI or MMC and which physical ports? I don't use onboard: gyroscope, magnetometer, lcd interface, touchscreen interface.
2022-03-13 5:55 AM
One could perhaps check schematic vs data sheet to see if you've got any hope of exposing the SDMMC interfaces.
SPI should at least be exposed on the Arduino rails.