cancel
Showing results for 
Search instead for 
Did you mean: 

Buffer error after debug in the variable field there is an error message uint8_t buff_tx[10] = {11,12,13,14,15,16,17,18,19,20}; program was taken from you tube link : https://www.youtube.com/watch?v=xE6GVt7XuJI

RKore.1
Associate II

buff_tx Error: Multiple errors reported.\ Failed to execute MI command: -var-create - * buff_tx Error message from debugger back end: -var-create: unable to create variable object\ Failed to execute MI command: -var-create - * buff_tx Error message from 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Perhaps you can show or attach your code. The output from the build process, debugging, etc.

Indicate what STM32 part/board you're actually using.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
RKore.1
Associate II

Yes i can send the project

Can you send an address to send to

Thanks Tesla

I attach the project

Nucleo 429zi

Regards

Raz Koren