cancel
Showing results for 
Search instead for 
Did you mean: 

AP configuration

manuele
Associate
Posted on March 06, 2015 at 14:45

Hi, I have update SPWF01S firmware at 3.3version and now I need to create a AP with WPA protection.

I read in other post who the WPA setting is not supported for AP application, so AP is supported only by WEP standard? 

I try to enter with my smartphone in my net with WEP protection but I can't. ''0'' is the default password? How I set a new WEP password?  

I attach my statistic and variabiles:

+WIND:28:Station F4:09:D8:4A:59:CC Associated

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01SA

#  nv_serial = 1613D16031

#  nv_wifi_macaddr = 00:80:E1:FF:8C:45

#  blink_led = 0

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 115200

#  console1_hwfc = 0

#  console1_enabled = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 73:65:72:61:66:69:6E:69:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 8

#  wifi_channelnum = 6

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 3

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 1

#  wifi_wep_keys[0] = E5:92:D2:86:40:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 04:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wpa_psk_text =

#  ip_use_dhcp = 1

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-FF-8C-45

#  ip_apdomainname = captiveportal.net

#  ip_ipaddr = 255.255.255.255

#  ip_netmask = 255.255.255.255

#  ip_gw = 255.255.255.255

#  ip_dns = 255.255.255.255

#  ip_http_get_recv_timeout = 3000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

OK

+WIND:72:Station F4:09:D8:4A:59:CC Disassociated:8

# Status & Statistics:

#  version = 141106-0950875-SPWF01S

#  reset_reason = 2

#  conf_flag = 5

#  system_uptime = 214

#  system_sleeptime = 0

#  gpio_enable = 0

#  captiveportal = 1

#  wifi_state = 10

#  wifi_bssid = 00:80:E1:FF:8C:45

#  wifi_aid = 0

#  wifi_channelnum = 6

#  wifi_sup_rate_mask = 0x003FFFCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_chan_activity2 = 0x00000040

#  wifi_max_tx_power = 18

#  wifi_reg_country =

#  wifi_dtim_period = 0

#  wifi_sleeping = 1

#  wifi_num_assoc = 0

#  ip_ipaddr = 172.31.69.1

#  ip_netmask = 255.255.255.0

#  ip_gw = 172.31.69.1

#  ip_dns = 208.67.222.222

#  ip_sock_open = 0

#  ip_sockd_port = 0

#  free_heap = 21752

#  min_heap = 21504

#  current_time = 2327

The ''captiveportal.net'' function is possible to disable?

thanks you
1 REPLY 1
Posted on March 07, 2015 at 10:30

Hi Manuele,

from your confi dump, I see:

#  wifi_wep_keys[0] = E5:92:D2:86:40:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 04:00:00:00

it seems that wifi_wep_key_lens is not matching actual key length.

About captiveportal, what do you mean by disable its?

- Since miniAP's default IP address is randomly generated (when ''ip_use_dhcp'' is 1) starting from its MAC address, addressing captiveportal allows you to avoid knowing real miniAP IP address. Obviously you can change this symbolic address by ''ip_apdomainname'' variable.

- Another option, only valid for miniAP, you can set ''ip_use_dhcp'' variable to 2, and set miniAP default IP address. This way, captiveportal.net can be ignored.

- Last hint, only valid for miniAP: default homepage (index.html) is automatically redirected to ''firstset.html''. To recall default index.html, use ''captiveportal.net/index.html''.

Let me know if it helps you

jerry