2015-03-06 5:45 AM
Hi, I have update SPWF01S firmware at 3.3version and now I need to create a AP with WPA protection.
I read in other post who the WPA setting is not supported for AP application, so AP is supported only by WEP standard? I try to enter with my smartphone in my net with WEP protection but I can't. ''0'' is the default password? How I set a new WEP password? I attach my statistic and variabiles:+WIND:28:Station F4:09:D8:4A:59:CC Associated# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01SA# nv_serial = 1613D16031# nv_wifi_macaddr = 00:80:E1:FF:8C:45# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 0# console1_enabled = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval = 100# wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = 73:65:72:61:66:69:6E:69:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 8# wifi_channelnum = 6# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 3# wifi_auth_type = 0# wifi_atim_window = 0# wifi_powersave = 0# wifi_tx_power = 18# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 1# wifi_wep_keys[0] = E5:92:D2:86:40:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 04:00:00:00# wifi_wep_default_key = 0# wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wpa_psk_text =# ip_use_dhcp = 1# ip_use_httpd = 1# ip_mtu = 1500# ip_hostname = iwm-FF-8C-45# ip_apdomainname = captiveportal.net# ip_ipaddr = 255.255.255.255# ip_netmask = 255.255.255.255# ip_gw = 255.255.255.255# ip_dns = 255.255.255.255# ip_http_get_recv_timeout = 3000# ip_dhcp_timeout = 20# ip_sockd_timeout = 250OK+WIND:72:Station F4:09:D8:4A:59:CC Disassociated:8# Status & Statistics:# version = 141106-0950875-SPWF01S# reset_reason = 2# conf_flag = 5# system_uptime = 214# system_sleeptime = 0# gpio_enable = 0# captiveportal = 1# wifi_state = 10# wifi_bssid = 00:80:E1:FF:8C:45# wifi_aid = 0# wifi_channelnum = 6# wifi_sup_rate_mask = 0x003FFFCF# wifi_bas_rate_mask = 0x0000000F# wifi_chan_activity2 = 0x00000040# wifi_max_tx_power = 18# wifi_reg_country =# wifi_dtim_period = 0# wifi_sleeping = 1# wifi_num_assoc = 0# ip_ipaddr = 172.31.69.1# ip_netmask = 255.255.255.0# ip_gw = 172.31.69.1# ip_dns = 208.67.222.222# ip_sock_open = 0# ip_sockd_port = 0# free_heap = 21752# min_heap = 21504# current_time = 2327The ''captiveportal.net'' function is possible to disable?thanks you2015-03-07 1:30 AM
Hi Manuele,
from your confi dump, I see:# wifi_wep_keys[0] = E5:92:D2:86:40:00:00:00:00:00:00:00:00:00:00:00
# wifi_wep_key_lens = 04:00:00:00
it seems that wifi_wep_key_lens is not matching actual key length.About captiveportal, what do you mean by disable its?- Since miniAP's default IP address is randomly generated (when ''ip_use_dhcp'' is 1) starting from its MAC address, addressing captiveportal allows you to avoid knowing real miniAP IP address. Obviously you can change this symbolic address by ''ip_apdomainname'' variable.- Another option, only valid for miniAP, you can set ''ip_use_dhcp'' variable to 2, and set miniAP default IP address. This way, captiveportal.net can be ignored.- Last hint, only valid for miniAP: default homepage (index.html) is automatically redirected to ''firstset.html''. To recall default index.html, use ''captiveportal.net/index.html''.Let me know if it helps youjerry