cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L8CX - Range Data Preprocessing designed for mobile phone requirments

Paul_Anthony
Associate II

I just wanted to check the validity of an old post from 2022.

The VL53L8CX, like other TOF devices returns a 8x8 grid of distances.

The distances are tuned, so if a flat surface for example a wall is directly in front of the sensor (sensor is facing the wall with no offset or rotation) at a distance of 1 metre. Then all the 8x8 Zones will report a distance of 1 metre (assuming no floor, ceiling etc..., so there are no other reflections etc...). The measured distances are in fact larger for angles offset from zero, but they compensated for the requirements of the mobile phone manufacturers etc... 

Is this still true. 

Link to post:-

Solved: VL53L5CX Distances Don't Match Theory - What am I ... - STMicroelectronics Community

1 ACCEPTED SOLUTION

Accepted Solutions
Anne BIGOT
ST Employee

Hello 

The post from 2022 is still valid.

Like for other sensors, all the 8x8 zones will report the same distance and there is a compensation due to the angles.

Anne 


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'

View solution in original post

1 REPLY 1
Anne BIGOT
ST Employee

Hello 

The post from 2022 is still valid.

Like for other sensors, all the 8x8 zones will report the same distance and there is a compensation due to the angles.

Anne 


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'