2024-06-11 7:43 PM
I am looking to purchase an evaluation board for the VL53L8CH in order to take advantage of the CNH data for potential use in AI models.
The below expansion board web page has the below text (Link below)
I already have a VL53L8CX, which lacks the CNH data. The info on the web page has both part numbers, however I think only the VL53L8CH has the functionality I require.
This is just the expansion board. I guess the main board could be the following board.
This page has the main board and expansion board.
Hopefully this should be ok for assessment of the VL53L8CH.
My company is based in Japan, so the plan is to order it within the next week.
Solved! Go to Solution.
2024-06-12 12:44 AM
Hello
To evaluate the VL53L8CH you need to purchase the main board + expansion board. The best is to purchase the P-NUCLEO-53L8A1.
If you already have a NUCLEO-F401 you can only purchase the X-NUCLEO-53L8A1
The same X-NUCLEO-53L8A1 can be used to evaluate both VL53L8CX and VL53L8CH.
Anne
2024-06-12 12:44 AM
Hello
To evaluate the VL53L8CH you need to purchase the main board + expansion board. The best is to purchase the P-NUCLEO-53L8A1.
If you already have a NUCLEO-F401 you can only purchase the X-NUCLEO-53L8A1
The same X-NUCLEO-53L8A1 can be used to evaluate both VL53L8CX and VL53L8CH.
Anne