VL53L7CX Driver - Implement from VL53L5CX driver?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-12 2:52 AM - last edited on ‎2024-08-12 8:16 AM by Peter BENSCH
Hi,
I have implemented the VL53L5CX driver for a Nordic controller, and it works fine.
Now, I want to implement the VL53L7CX driver for the same Nordic controller.
Can I use the VL53L5CX driver as is, or will I need to make changes?
Additionally, are there any hardware modifications required, or can I use the same hardware as with the VL53L5CX?
Solved! Go to Solution.
- Labels:
-
Time of flight
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-12 3:03 AM
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-12 3:03 AM
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-12 4:20 AM - edited ‎2024-08-12 5:57 AM
Hi,
so where i want to write
uint8_t fw_flags[8];
status |= vl53l5cx_dci_read_data(&Dev, fw_flags, 0xE0C4, sizeof(fw_flags));
printf("Module type = %u (0 for vl53l5cx, 1 for vl53l7cx)\n", fw_flags[1]);
after init or before init of vl53l7cx?
using hardware it is possible to change the vl53l7cx address?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-12 7:35 AM
The L5 and the L7 are identical bits of silicon. They only differ in the Field of View - which is a diffuser and lens change.
Prior to boot, only the I2C interface is active, so issuing a complex DCI read is not going to work. One should do the Init first. Then issue your DCI read.
As for changing the I2C address, use this procedure:
Put all sensors in LPn =0.
Bring the first one to LPn=1.
Do the init.
issue the address change command.
Update your address structure to access that chip at the new address.
Bring up the next sensor and repeat the process of LPN=1, init, address change, update structure.
Technically you don't have to change the address on your last sensor, but I do it anyway.
That way i can access the default address. If any of the chips have rebooted (due to lost power or something) they will again respond on the default address.
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.