2023-09-27 12:34 AM
Hi,
I am struggling to understand how to calculate the load capacitance when adding the pull-up resistors in my circuit with VL53L4CD ToF sensor to run the sensor in fast mode plus. The datasheet states that:
Suggested pull-up and series resistors for I²C fast mode plus
I²C load capacitance (CL)(1) Pull up resistor (Ohms) Series resistor (Ohms)
CL ≤ 90 pF 1.5 k 100
90 pF < CL ≤ 140 pF 1 k 50
140 pF < CL ≤ 270 pF 0.5 k 50
270 pF < CL ≤ 400 pF 0.3 k 50
1. For each bus line, CL is measured in application PCB by customer.VL53L4CD
I am using a NUCLEO-F401RE evaluation board that is communicating and driving the ToF VL53L4CD-SATEL board.
Anybody can help with this? Thanks in advance.
2023-10-09 12:49 AM
Hello,
Your question has been raised internally. I will come back to you as soon as I have an answer.
Regards
Anne
2023-10-10 11:54 PM
Hi Anne, thank you. I will be looking forward to the feedback.
2023-10-11 5:57 AM
Hello,
We have one AN that could be interesting for you.
It is AN5837 which explains how to connect the SATEL to the Nucleo board.
Hope this helps,
Regards
Anne