cancel
Showing results for 
Search instead for 
Did you mean: 

ToF sensor with high Signal count rate of 1MHZ

vishnusf
Associate III

Hi,

Can somebody please suggest me a ToF sensor with signal sampling rate of atleast 1MhZ.

 

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions

The ToF sensors from STMicroelectronics measure the propagation time of the photons from the integrated laser to the integrated receiver using a proprietary method. An ADC would be far too slow for the short propagation times, which is why there is no sampling rate.

The ToF sensors also cannot work with external lasers.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
John E KVAM
ST Employee

Sorry - 

I don't know of an ST part that can help you. 

-john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Peter BENSCH
ST Employee

@vishnusf

  • What do you want to use a ToF sensor (time-of-flight) for?
  • Why are you interested in a sampling rate that has nothing to do with ToF sensors, but with ADCs?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

HI Peter,

Thanks for the reply.

  • What do you want to use a ToF sensor (time-of-flight) for?                                                                                            We want to use for a biomedical application. We plan to use an external continuous laser with the sensor.
  • Why are you interested in a sampling rate that has nothing to do with ToF sensors, but with ADCs?                     We need to know the sampling frequency since our application uses fourier transfrm hence we need the sampling rate of the signal.

The ToF sensors from STMicroelectronics measure the propagation time of the photons from the integrated laser to the integrated receiver using a proprietary method. An ADC would be far too slow for the short propagation times, which is why there is no sampling rate.

The ToF sensors also cannot work with external lasers.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.