cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-IMG031 linux driver for VL53L4CX hosted anywhere?

jgsandom
Associate

Hi there,

We want to use the VL53L4CX ToF sensor and I want to build the out of tree kernel module for the STSW-IMG031 (here) via Yocto recipe. Are the sources hosted anywhere on Github or elsewhere so I can clone the repo directly via Yocto rather than having to download the sources and add it to a private Github?

I've seen this SVN link on one of the docs in the driver package but could not access it via subversion - has the repo moved?

http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3/

 

svn checkout http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3                                                                                                                    
svn: E170013: Unable to connect to a repository at URL 'http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3'
svn: E670002: Name or service not known

Thanks,

Joe

 

1 REPLY 1
Anne BIGOT
ST Employee

Hello

The svn repo mentionned above is an internal release and should not appear in there. 
We will clean it. 

Regarding git, the linux driver is not yet available under any GitHub. Sorry for that.

Regards

Anne


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'