cancel
Showing results for 
Search instead for 
Did you mean: 

Static library for Smart Presence Detection compatible with Android (both 64-bit and 32-bit)

yogesh3699
Associate

Hi,

 

Could you provide the static library for Smart Presence Detection compatible with Android (both 64-bit and 32-bit), as well as ARM Linux (both 64-bit and 32-bit)?
 
3 REPLIES 3
Joe WILLIAMS
ST Employee
Hi yogesh3699 This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly. Kind Regards Joe WILLIAMS STMicro Support
John E KVAM
ST Employee

This is a little tricky. One has to compile a library not for 'android' or 'linux' but for the particular CPU (or MCU). Our existing libraries are for Arm Cortex processors - because that's what the STM32 is based on. If you want a different CPU, one pretty much as to specify which CPU it is. 

It's also tricky because unless someone has to dig up a cross-compiler. Not impossible, but not easy either. 


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Anne BIGOT
ST Employee

Hello,

The libraries were added on st.com in the STSW-IMG048 revision 1.0.1

You can find them in the SmartPresenceDetectionKit_LnA_1.0.0 direcotry.

 


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'