2022-06-13 4:12 AM
Hello,
The physical infrared filter give some faulty measurements and wont stick perfektly on the VL53L5CX.
kind regards
Maik H.
Solved! Go to Solution.
2022-06-17 4:36 AM
This liner is put to protect the sensor from soldering.
To use the sensor, you have to remove the liner. If you use the sensor with it, it explains your faulty measurements.
2022-06-17 1:32 AM
Hello,
What do you mean by physical infrared filter ? Is it the liner on top on the sensor ?
Indeed, the physical infrared filter is inside the sensor.
Regards
2022-06-17 3:20 AM
Hello,
Thank you for your reply.
I mean the little foile on top of the VL53L5CX like in the picture below.
kind regards
Maik H
2022-06-17 4:36 AM
This liner is put to protect the sensor from soldering.
To use the sensor, you have to remove the liner. If you use the sensor with it, it explains your faulty measurements.
2022-06-17 4:41 AM
Thank you for your reply,
so in this case i can use it safe without this protect foile?
Kind regards
Maik H
2022-06-17 4:49 AM
Yes that's safe. No worry.
Regards
Anne