2023-05-17 02:09 PM
The calibration procedure for a VL6180X sensor states that the offset calibration does not need to be done if the sensor is within +/- 3mm for a specified target. Is there every a situation in which the cross-talk calibration procedure doesn't need to be performed?
Can ambient light impact my offset and cross-talk calibration values?
2023-05-18 03:47 AM
Hi BMcGe
Cross-talk is the the TOF emitted light bounce back from glass to receiver, so cross-talk calibration is needed if you add a cover glass on top of VL6180CX.
Ambien light contain 850nm light will affect calibration result, if the light doesn't have 850nm energy, there will be no risk.
Br
Zhiyuan.Han
2023-05-18 08:02 AM
Would calibrating the cross-talk when there is no cover glass cause any issues with the sensor's readings?