cancel
Showing results for 
Search instead for 
Did you mean: 

Does the cross-talk calibration on a VL6180X sensor always need to be performed?

BMcGe.1
Associate II

The calibration procedure for a VL6180X sensor states that the offset calibration does not need to be done if the sensor is within +/- 3mm for a specified target. Is there every a situation in which the cross-talk calibration procedure doesn't need to be performed?

Can ambient light impact my offset and cross-talk calibration values?

2 REPLIES 2
Zhiyuan.Han
ST Employee

Hi BMcGe

Cross-talk is the the TOF emitted light bounce back from glass to receiver, so cross-talk calibration is needed if you add a cover glass on top of VL6180CX. ​

Ambien light contain 850nm light will affect calibration result, if the light doesn't have 850nm energy, there will be no risk.

Br

Zhiyuan.Han


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BMcGe.1
Associate II

Would calibrating the cross-talk when there is no cover glass cause any issues with the sensor's readings?