2021-03-23 9:39 AM
Please, do you know if there is a way to solve stability problems with the VL53L1X satel ?
Thank you for your help.
Best wishes
Anne
Solved! Go to Solution.
2021-08-19 10:56 AM
That satel board and the I2C connection are really touchy.
I'm going to guess that if you have more than 6 or 8 inches of wire, you are going to run into this problem.
Try seperating the wire and twisting it. Or use thicker wire.
The right answer are stronger pull-ups, but that's a lot of work.
2021-08-19 10:56 AM
That satel board and the I2C connection are really touchy.
I'm going to guess that if you have more than 6 or 8 inches of wire, you are going to run into this problem.
Try seperating the wire and twisting it. Or use thicker wire.
The right answer are stronger pull-ups, but that's a lot of work.