2024-06-18 1:43 AM - edited 2024-06-18 2:15 AM
Hello,
I'm trying to get a VL6180X sensor to work.
I've downloaded the latest API: en.VL6180_API_V1.3.0.zip
My goal is to make the sensor work in I2c on a Raspberry PI in the c or c++ language.
But I can't compile my code, or rather compile the api into a library.
Where can I find an example of a makefile or command to do this?
Thanks for your help.
2024-06-18 2:04 AM - edited 2024-06-18 2:23 AM
Did you mean to ask a question?
EDIT: OP has now been updated to include a question
2024-06-18 2:22 AM
@SCADE wrote:But I can't compile my code, or rather compile the api into a library.
What problem(s), exactly, are you facing?
What have you tried so far?
Again, please see:
2024-06-18 2:41 AM
Ok so here is my test.cpp file :
#include <iostream>
#include <unistd.h>
#include "vl6180_api.h"
int main()
{
VL6180Dev_t tof = 0x29;
VL6180_WaitDeviceBooted(tof);
VL6180_InitData(tof);
VL6180_Prepare(tof);
for (size_t i = 0; i < 10; i++)
{
VL6180_RangeData_t rangeData;
VL6180_RangePollMeasurement(tof, &rangeData);
printf("Range: %d\n", rangeData.range_mm);
}
VL6180_FilterSetState(tof, 1);
return 0;
}
file structure :
api_vl6180x_1.4.0/
api_vl6180x_1.4.0/config
api_vl6180x_1.4.0/config/vl6180_cfg.h
api_vl6180x_1.4.0/core
api_vl6180x_1.4.0/core/inc
api_vl6180x_1.4.0/core/inc/vl6180_def.h
api_vl6180x_1.4.0/core/inc/vl6180_api.h
api_vl6180x_1.4.0/core/src
api_vl6180x_1.4.0/core/src/vl6180_api.c
api_vl6180x_1.4.0/platform
api_vl6180x_1.4.0/platform/template
api_vl6180x_1.4.0/platform/template/vl6180_platform.h
api_vl6180x_1.4.0/platform/template/vl6180_types.h
api_vl6180x_1.4.0/platform/cci-i2c
api_vl6180x_1.4.0/platform/cci-i2c/vl6180_i2c.c
api_vl6180x_1.4.0/platform/cci-i2c/vl6180_i2c.h
and finally compile command :
g++ -o test test.cpp api_vl6180x_1.4.0/core/src/*.c api_vl6180x_1.4.0/platform/cci-i2c/*.c -I api_vl6180x_1.4.0/core/inc/ -I api_vl6180x_1.4.0/platform/template/ -I api_vl6180x_1.4.0/config/ -lwiringPi
Error :
/usr/bin/ld: /tmp/ccnVF5wY.o: in function `VL6180_WaitDeviceBooted':
vl6180_api.c:(.text+0x6c): undefined reference to `VL6180_RdByte' ......................................
2024-06-18 2:52 AM - edited 2024-06-18 3:03 AM
@SCADE wrote:Error :
/usr/bin/ld: /tmp/ccnVF5wY.o: in function `VL6180_WaitDeviceBooted':
vl6180_api.c:(.text+0x6c): undefined reference to `VL6180_RdByte' ......................................
"undefined reference" is a linker error.
It means that you have omitted to provide a definition of that function - either as source code, or as a pre-built binary library.
Probably, you have #included a header which just declares that function (ie, just provides a prototype) - hence the compiler is happy - but haven't added the necessary source or pre-built binary library to your project - so the link fails.
#UdefinedReference
EDIT:
Looks like these are the docs you need:
2024-06-18 3:25 AM - edited 2024-06-18 3:26 AM
This is also what I understand the definition seems to be missing, however it is present in
for VL6180_RdByte :
Function declaration: vl6180_api.h
Function definition: vl6180_i2c.c
Function usage: vl6180_api.c
And I seem to be integrating them all correctly in my compile command
2024-06-18 7:37 AM
When we write the code you are using, we don't know what MCU ( or CPU) you have.
So, we write the code all the way to RdByte() and WrByte() and then WE STOP.
It's up to you to populate those functions.
Have a look at the platform.c function and Platform.h
Notice they are basically empty?
There are examples of VL6180 projects on Linux - on GitHub.
Download one of those and borrow the Platform.c file.
You basically have to insert a IOCTL I2C write function into RdByte().
- john
2024-06-19 5:51 AM
Thanks for your reply,
The API documentation recommends using cci-i2c (should work on raspberry??)
In the files of the cci-i2c folder there are the functions you say are missing but that I can't get to work ;(
And on Github I couldn't find anything relevant.