Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX custom ranging grid

I see that the ultralite driver for the VL53L5CX supports 4x4 60Hz and 8x8 15Hz, but my use case would really benefit from a custom ROI set like the VL53L1 was able to use (in this case I'd like to do an 8x2 grid covering the two central bands of the...

Resolved! Multiple byte read for VL53L5CX?

We seem to be having trouble getting through the vl53l5cx_init(&Dev); function for the VL53L5CX. We can read single bytes but multiple byte (4) reads trigger the TIMEOUT and the ULD doesn't load successfully. Here is our RdMulti function:uint8_t RdMu...

KWine by Senior
  • 2362 Views
  • 3 replies
  • 0 kudos

Resolved! [VL53L3CX]The RAM DATA is too big in STSW-IMG015's example code

The VL53L3CX API‘s example code use 12KB of RAM, which makes it impossible for me to try to use the program with a smaller RAM MPU.The example for L1X,L0 are not the same, they only use about 2KB of RAM.I would like to know if it is necessary to use ...

YChen.9 by Associate II
  • 1103 Views
  • 1 replies
  • 0 kudos

Resolved! Distance to different SPAD zones in VL53L1X sensor

Hello, I have series of questions related to the data implementations using SPAD zone settings. After reading of manuals i made conclusions how to use this feature of the sensor, but i'm not sure if my conclusions are correct.1. I'm interested in acc...

AShmy.1 by Associate
  • 1673 Views
  • 1 replies
  • 0 kudos