Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

about GUI installation for X-NUCLEO-53L1A1

We bought P-NUCLEO-53L1A1 for testing the performance of VL53L1X.We met some trouble for setup and software installation.According to the Quick Start Guide for X-NUCLEO-53L1A1), we tried toinstall VL53L1X GUI to our PC, but failed. Attached images f...

DSai.1 by Associate III
  • 1145 Views
  • 2 replies
  • 0 kudos

Resolved! vl53l1x shortest distance measurement

I have a vl53l1x and testing it without glass and uncalibrated operating in SHORT distance mode. I get distance measurements of non-zero values at about 120mm. The datasheet claims 4cm. Will the calibration process result in short measurements inline...

WMaho.1 by Associate
  • 1595 Views
  • 1 replies
  • 0 kudos

VL53L5CX - Several sensors in parallel

I worked with a single VL53L5CX under Linux without problems. Now I wan't to have at least two sensors running in parallel connected to the same I2C bus. So I followed the documentation and first set LPn for the sensor which should keep its address (...

PBoer.1 by Associate II
  • 1464 Views
  • 1 replies
  • 0 kudos

Daisy chain multiple VL53l1X - lack of information about GPIO1

Hello,due to the bad datasheet and missing register map it is almost impossible to get information about GPIO1. The only settings i found are affecting the interrupt functionality. But why is the pin called GPIO when only used as interrupt output. Sh...

MStoc.1 by Associate
  • 1245 Views
  • 2 replies
  • 0 kudos