cancel
Showing results for 
Search instead for 
Did you mean: 

Background Noise using SPAD array

shjayago
Associate

Heya, 

 

Is it possible to see the background light (intensity/histogram) without actually transmitting, using a VL53L8 or VL53L9?

We don't want to measure the distance to objects. We just want to be able to use the SPAD array to get histogram for each zone. 

Its a high volume use-case, so would be great if we can achieve this.

 

regards

Shjayago

3 REPLIES 3
AScha.3
Chief III

Hi,

just to see the background light - why you dont use a device , that's built for this : a cheap camera/video chip ?

If you feel a post has answered your question, please click "Accept as Solution".
John E KVAM
ST Employee

An interesting question. Although I can't imagine what you would get. That histogram is created by turning on the VCSEL maybe a million times, catching a bunch of photons after every flash and building up the bin data.

I don't think the histogram would have any meaning if you just started capturing photons.

ST makes the SPAD array and we would be overjoyed to build an array for you. Initial cost is kind of high though. 

I think it's a million or two dollars for the first 5 wafers. 

So it has to be a REALLY high volume application to make it worth it. 

The thing that makes this chip work is the tight coupling of the VCSEL driver and the SPAD array. I'm afraid if you decoupled these elements, it would be extremely hard to get the timing right. 

But if that is what you really wanted to do, I expect we could find some way to disable the VCSEL.

If you think you have a good shot at an innovative product, go to the community page, click on support and find a someone in sales. They can and will get you to a marketing person who can explain how to go about the next steps. 

- john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
RogerM
ST Employee

Shjayago,
The VL53L8 can output the ambient-light-level-per-zone, this is the background light level seen between VCSEL pulses. Is this what you want? There is no histogram associated with this data, it is just a single value per zone.

However, you do need to run the device in ranging mode to get this data out i.e. the VCSEL will be active between the ambient level measurements. But if all you are interested in is the ambient level data you can set the integration time, i.e. the active ranging period, to a short period to minimise the power used.

Roger