Sorry, I am not entirely sure what is expected in the screen shots.But I can make a few general comments.The basic histogram bin width in terms of difference-of-target-range-per-bin is about 37mm per bin. So it is very hard to determine accurate ran...
VHV is an internally generate voltage used within the SPAD array. So it is not affecting VCSEL power and should not be affected by external supply voltage variations.VHV calibration makes small changes to this voltage to stabilise the SPAD sensitivi...
Have you found pages 33 to 36 of the MZAI_EVK User Manual ?You can use the cnhMergeX and cnhMergeY parameters to combine zones into a lesser number of aggregates.For instance, running in 4x4 mode you can combine all the 16 zones into a single aggrega...
The preset "Zone 8x8" configuration only uploads standard zone target data (i.e. target range, signal etc.).You need to select one of the 'CNH xxxx' presets to see the histogram data.ExtendedMode=2 is needed to output CNH histogram data.ExtendedFlag...
Basic configuration of the device mode is done via:ResolutionRangingPeriodIntegrationTimeConfiguration of what histogram data to capture is done with:cnhStartXcnhStartYcnhMergeXcnhMergeYcnhColscnhRowscnhNumBinscnhStartBincnhSubSampleWhat data to uplo...