cancel
Showing results for 
Search instead for 
Did you mean: 

Using A-GNSS to improve TTFF

carl239955
Associate II

Hello 

I am interested at looking at the Teseoo-LIV3F for a application but I require a very fast TTFF. Having read up on the A-GNSS option will this be available any where or any location in the world as long as the server is accessible ?

So no matter where you are as long as you can access the A-GNSS server the TTFF speed should improve considerably from up to 35s for COLD START to a few seconds after accessing and relaying the relevant data / information ?. The ephemeris data obtained from the server will be valid for your location and your sky ?

 

thanks

 

cab

1 ACCEPTED SOLUTION

Accepted Solutions
3 REPLIES 3
Francesco Virlinzi
ST Employee

Hi 

with LIV3F supports you have the autonomous AGNSS (which doesn't need any extra data)... the modules will learn the satellites orbit and it will use the prediction to provide a fast TTFF.

The Real-Time AGNSS is based on data coming on the internet server and it's for free on LIV3F. From the server you will download all the satellites information for all locations

Thank you Francesco - is there an App note on this feature ?

Hi

On Autonomous AGNSS there is no AN (but it's enabled by default in the module)

On Real-Time AGNSS you can have a look at:

https://www.st.com/resource/en/application_presentation/teseo-3-quick-testing-guide.pdf

https://www.st.com/resource/en/application_note/an5160-rxnetworks-assisted-gnss-server-interface-specification-stmicroelectronics.pdf

Regards

 Francesco