2023-12-12 01:25 AM
Hello,
Is there any specific parameters to configure to acheive correct CEP?
Starting from default mode I found a CEP worst than some L1 only GNSS....despite I respect the 70x70mm ground plan for the antenna....
Many points are correct (but not more) but a few are awfull (more than 20m far away from position...)
Do you suggest any ceramic antenna?
Best regards
Mich
2023-12-18 01:26 AM
Hi
In the Teseo-Suite configuration, did you 'NMEA 4.x' as protocol parser?
Regards
Francesco
2023-12-18 02:14 AM
Hi,
NO when I select NMEA 4.X the the signal level tool does not work!
Only the the view monitoring works correctly....
Do you have any other suggestion please?
Best regards
Mich
2023-12-18 02:23 AM
Hi
LIV4F as multi-bands device provides a NMEA-4.x ASCII stream.
Which Teseo-Suite version are you using?
In any case in the ASCII stream you can see if BeiDou/Galileo etc are acquired or not.
Regards
Francesco
2023-12-18 02:44 AM
Teseo Suite Pro 7.0.3.0 (downloaded last week)
I see GL, GA, GP and BD talkers for GSV messages
2023-12-18 02:51 AM
Hi
I'm using the same Teseo-Suite version (7.0.3.0)
LIV4F firmware version 4.6.3.5.3)
and teseo-suite parses the NMEA4.x from LIV4F without any issue.
BTW :
> GL, GA, GP and BD talkers for GSV messages
The module is correctly acquiring the GPS, Galileo, BeiDou constellation.
Regards
Francesco
2023-12-18 09:29 AM
So with the GNSS on the car roof on a parking and a test on 15mn I have a CEP of 2.3m.
Do you have advices to improve this?
As you can see sudenly latitude and longitude changed despite the GNSS did not moved...