2023-08-23 10:33 AM
What is the timing specification of the PPS (Pulse Per Second) output from the Teseo-LIV3R in terms of pulse width and/or duty cycle? I've reviewed the datasheet, UM2523 (ST Teseo III ROM binary image - User manual), and UM2231 (Teseo-LIV3 GNSS Modules - Hardware Manual) but don't see this specified.
2023-08-23 11:05 AM
There are parameters and settings you can read out.
For the docs looks to be 1 Hz 50/50 duty, quantization probably +/-16ns
2023-09-05 1:51 PM
Hi Tesla DeLorean,
Thanks for the replying to my question. In which document did you find this information?
2023-09-12 11:00 AM
Hi Tesla DeLorean,
I'm not sure if you saw my question from last week. You wrote "For the docs looks to be 1 Hz 50/50 duty, quantization probably +/-16ns" but I can't find the document that specifies this. Would you please tell me where you found this specification?
Sincerely,
Hal
2025-01-08 7:53 AM
Additional question, is it the rising edge or the falling edge that is synchronized to the second rollover?
2025-01-15 8:36 AM
Hi,
For timing applications, I would consider using Teseo LIV3FL.
You can adjust the pulse duration (time from rising to falling edge) of the PPS signal by changing CDB-301.
Datasheet https://www.st.com/resource/en/datasheet/teseo-liv3fl.pdf
You can find the link to Software manual here.
LIV3FL has same pinout of LIV3R but LIV3FL can do 3 constellations and is a flash based device.