2019-10-30 7:54 AM
2019-10-30 8:05 AM
Hi
Did you change anything in the firmware configuration?
Which tool are you using? EVB-LIV3F or X-Nucleo-GNSS?
Thanks
Regards
Francesco
2019-10-30 8:20 AM
Yes, I tried to configure the firmware. But the process freezes and Teseo no longer communicates with the PC.
No I do not use VB-LIV3F or X-Nucleo-GNSS.
I have a Teseo module soldered to the board.
2019-10-30 8:26 AM
From your MCU-host you should perform a firmware-update where the configuration is removed.
You can take the firmware @ https://www.st.com/content/st_com/en/products/embedded-software/automotive-infotainment-and-telematics-software/teseo-liv3fsw.html
Take care that to perform firmware-update your MCU has to driver the Teseo-LIV3F.nReset pin.
Just a question: what were you configuring? may be it's just a baud-rate issue?
Did you see PPS blinking? May you can communicate with I2C port.
Regards
Francesco
2019-10-30 1:37 PM
But can I complete firmware-update where the configuration is removed from the PC and terminal program or using any other program?
2019-10-30 1:40 PM
speed did not change exactly
Worked only on UART, PPS is not possible to control.
2019-10-31 1:13 AM
Hi
Firmware update is always possible because internally it doesnt' care on the configuration.
On the PC:
On the board:
On Module reset the firmware update will start.
Hope this helps
Regards
Francesco
2019-11-03 11:39 PM
Hi
So that's the point, Teseo-Suite throws an error when you press the STA808x / 9x FW Upgrade button in the Tools menu?
2019-11-04 1:10 AM
2019-11-04 1:41 AM
Hi
thanks for the help
version of Teseo-Suite - 5.2.3.4
install Teseo-Suite as Administrator