cancel
Showing results for 
Search instead for 
Did you mean: 

the coordinates (latitude and longitude) of the Teseo-LIV3F

Iyaku
Associate II

Hi! Why are the coordinates (latitude and longitude) of the Teseo-LIV3F changing abruptly and not smoothly like the u-blox M8 and NV08? Smooth change of coordinates is very important to me, since the direction angle is calculated in our program precisely

0690X00000ArkH9QAJ.jpg0690X00000ArkGuQAJ.jpg

10 REPLIES 10
Francesco Virlinzi
ST Employee

Hi

More probably the Stop Detection algorithm is reducing the fix evaluation frequency.

You can try disabling it in the CDB-200 bit[15].

Hope this helps

Regards

Francesco

Hi

Thanks for the help!

I will try to check your advice.

What does the walking detection algorithm do?

Hi

Turned off the Stop Detection algorithm in the CDB-200 bit [15] - the end result has not changed, jumps in the track angle are observed. What else can be done?

0690X00000ArsvCQAR.jpg

Just a question looking the image...

Are you comparing devices with the same frequency FIX rate?

Are both the device running at 1 Hz FIX?

Thanks

Regards

Francesco

Hi

I compare devices with the same FIX frequency.

Both devices operate at 4 Hz FIX. Devices work on GPS, Galileo, Beidou.

UART 9600, NMEA RMC, and GGA output rates.

> Both devices operate at 4 Hz FIX. Devices work on GPS, Galileo, Beidou.

I did an experiment with your setting and I can see the CPU is 100% of it's time....

In our default CPU runs @ 48Mhz it seems not enough in your setting...

You can increase the CPU speed @ 196MHz with this commands:

> $PSTMSETPAR,1130,00,0

> $PSTMSAVEPAR

Regards

Francesco

I forgot to say, the frequency has already been set to 196 MHz.

> I forgot to say, the frequency has already been set to 196 MHz.

ok.

Could you try enabling the walking mode? It 's an optimization in case of low-speed.

Regards

Francesco