2024-12-19 12:53 PM
Hello everyone!
I'm a beginner in hardware design and I'm trying to design a simple smartwatch. For the GPS function I decided to use the Teseo-Liv3r. The fact is that in the user manual they indicate several types of antenna, in this case I have selected one of the recommended ones, the ANT1818B00BT1516S.
My questions are:
+ Section 8 is the recommended layout, it tells me to use a 50 ohm line, how can I calculate the track thickness correctly?
+ On the other hand, section 9.1.2 shows an example layout, does it maintain a specific distance between tracks?
+ I understand that surrounding the track path is to ensure the RF path, should I take into account that tracks pass under the path in other layers? Or, if there is a ground plane, would it not affect it?
Finally, do you think I should use another type of antenna for my design? I'm looking for something small, but I'm not sure which one to choose.
Thank you very much in advance
2024-12-20 7:04 AM - edited 2024-12-20 9:36 AM
Hi Natalia,
I have forwarded your question to our EMEA marketing and apps. I am not very knowledgeable in RF side, so would like our h/w engineer to guide you.
Since this is holiday break next week, please expect a delay in response. Apologize for the inconvenience.
Thanks,
George.