Subject | Author | Posted | |
---|---|---|---|
If my accelerometer ODR on the LSM6DSOX is set at 3333Hz and my FSM (104Hz) checks accelerometer no...
| 2022-06-26 08:42 PM | ||
2022-06-26 05:52 AM | |||
2022-06-26 01:41 AM | |||
Good morning. Up front I apologize if these questions are simplistic in nature but I just really wa...
| 2022-06-24 10:37 AM | ||
Basically I'm working on ISM330DLC for interfacing I have used ism330dlc_read_data_polling data exa...
| 2022-06-16 11:59 AM | ||
2022-06-13 09:22 AM | |||
I'm working on LSM6DSOX with our custom ARM Cortex M4 core with I3C master. I have few doubts a...
| 2022-06-08 02:30 AM | ||
I am running on linux and trying to collect accel and gyro samples from the IMU. I have configured ...
| 2022-05-23 11:56 AM | ||
Hello, I'm working on the "STEVAL-MKI182V2" mounted on the "STEVAL-MKI109V3" development board. ...
| 2022-05-18 01:55 AM | ||
I did a lot of trials: the raspian OS seems to have drivers problems because if I do a Google voice...
| 2022-05-17 02:23 AM | ||
Hello everyone, We are working on an Android 11 i.MX8MM based board which has the LIS3DH accel...
| 2022-05-16 11:56 PM | ||
I have measured an offset drift around 6 mm when I heat VL53L4CD sensor from 24ºC to 45ºC. In order...
| 2022-05-16 03:36 AM | ||
Greetings. We are developing a device that will be needed to detect a back and forth shaking motio...
| 2022-05-13 08:09 AM | ||
Hi, I am developing an application using the accelerometer LIS2DW12. I need detect the single an...
| 2022-05-11 07:48 AM | ||
2022-05-10 11:15 AM | |||
Hi, I'm using a board which embeds two ST MEMS: ism330dhcx and lis3mdl. I'm exploiting the MotionFX...
| 2022-05-10 11:14 AM | ||
PB3 and PB10 are enabled as I2C2_SDA and I2C2_SCL to connect to LIS2DH12 SDA and SCL, the i2c2 code...
| 2022-05-10 08:10 AM | ||
HI I am using STEVAL-MKI182v2 sensor connected to Nucleo-F446ZE Evaluation board and printing the...
| 2022-05-10 06:36 AM | ||
Hello, I'm currently using a ST SensorTile.box STEVAL-MKSBOX1V1 in Expert Mode (by writing the fir...
| 2022-05-09 10:41 AM | ||
if i set CTRL1 = 0x0 X_H=0x00 X_L=0x57 Y_H=0x00 Y_L=0x5E Z_H=0x3F Z_L=0x33 if i set CTRL1 ...
| 2022-05-09 04:35 AM |