Subject | Author | Posted | |
---|---|---|---|
Hi ST engineers, my project use LSM6SDLTR connect with TI chip by I2C. I already get the orginal da...
| 2022-10-11 03:11 AM | ||
Is the sampling rate of the X,Y axis different from the Z axis? I am trying to sample at 1kHz and I...
| 2022-10-10 11:29 PM | ||
I want to detect both single and double tap and distinguish between them. For example, if I tap the...
| 2022-10-10 05:17 PM | ||
The possible configurations of the accelerometer filters are clear: While the properties of th...
| 2022-10-01 05:24 PM | ||
Hello, We have found a non-expected behavior of the IMU system LSM9DS1 when is set with an accele...
| 2022-09-16 02:05 AM | ||
Hello, I'm facing issues when enabling LIS3DH click interrupt, AOI1 and AOI2 interrupts on INT2...
| 2022-09-16 12:17 AM | ||
Dear SIR, When FIFO mode is disable. And Polling mode is used. There is a bit DRDY_MASK in regi...
| 2022-09-14 06:47 AM | ||
Dear SIR, In my application is to use lsm6dsr gyro values. When the set is in stationary state,...
| 2022-09-13 07:39 AM | ||
Hello Support Team, I am working on the LIS2DW12 Sensor with Wake-up feature. Issue : Gettin...
| 2022-08-25 05:28 AM | ||
In I2C mode for the IIS3DWB device the datasheet says it only support single axis mode because I2C ...
| 2022-08-24 02:06 PM | ||
here is my circuit for the LSM9DS1 i used the code from sparkfun breakout moduel to test the boa...
| 2022-08-24 01:33 AM | ||
Hello, I'm using a LIS2DTW12, here the configuration : ODR 400Hz FIFO threshold on INT2 pus...
| 2022-08-23 03:41 AM | ||
2022-08-22 04:25 PM | |||
I need to connect four LSM9DS1 on a common SPI bus. (I2C won't work here---resources are not availa...
| 2022-08-19 10:35 AM | ||
2022-06-29 12:44 AM | |||
Hello, we are a company that works with forklift trucks, and we want to implement the LSM6DS3TR-C ...
| 2022-06-28 01:27 AM | ||
If my accelerometer ODR on the LSM6DSOX is set at 3333Hz and my FSM (104Hz) checks accelerometer no...
| 2022-06-26 08:42 PM | ||
2022-06-26 05:52 AM | |||
2022-06-26 01:41 AM | |||
Good morning. Up front I apologize if these questions are simplistic in nature but I just really wa...
| 2022-06-24 10:37 AM |