Subject | Author | Posted | |
---|---|---|---|
I have an accelerometer LIS2DH12 connected to my STM32 with I2C and it works fine. Now I changed to...
| 2022-05-07 03:08 AM | ||
I'm trying to connect to AWS for cloud logging but in the android app during setup I select "select...
| 2022-05-06 11:28 AM | ||
y-axis z-axis I am using IIS3DWB to collect the vibration data. When the chip is stationary,...
| 2022-05-05 05:43 AM | ||
Hi, I've configured the LSM6DSO with an NRF52. The NRF52 is able to use DMA and to trigger the S...
| 2022-05-05 12:39 AM | ||
Hello dear ST community, How can I get activated INT1 for 6D/4D recognition in IIS2DH? I looked...
| 2022-05-03 08:08 AM | ||
Hello, I'm in the evaluation stage of LSM6DSO sensor. I've got a SensorTile.Box module and running...
| 2022-05-02 10:56 PM | ||
I used the LIS2DTW12 adapter board (STEVAL-MKI190V1) with I2C communication. power supply: 3V Wi...
| 2022-04-28 07:31 PM | ||
Hi folks, I am using the LSM6DSO sensor and trying to output data via the pin 2 interrupt. I've...
| 2022-04-27 05:22 PM | ||
I'm using the STM32-F446RE Nucleo board. I am using PB1 and PB2 to trigger on the iis3dwb interrupt...
| 2022-04-27 10:51 AM | ||
We are currently implementing a LIS2DE12 accelerometer into a project, but we have issues where the...
| 2022-04-27 07:49 AM | ||
Hey :) Im trying to use LIV3F with F303RE board. I have trouble to configure the LIV3F. Can it ...
| 2022-04-22 06:39 AM | ||
2022-04-15 06:45 AM | |||
Hello! Our application uses accelerometer in three modes: power down motion detection tilt ang...
| 2022-04-15 04:53 AM | ||
Hello, I am trying to set up an FSM on the LSM6DSO, but I have been struggling for several weeks...
| 2022-04-11 11:38 AM | ||
Hello everyone, I am currently looking at the IIS2MDC and the LSM303AGR and I wanted to know what ...
| 2022-04-11 07:25 AM | ||
i am trying to read the WHO_AM_I (read only) register and transmitting the data ( 0x0F | 0x80...
| 2022-04-08 07:13 AM | ||
2022-04-06 12:22 AM | |||
Configured the sensor ISM330DLC to capture 6.6KHz vibrations (which is max limit for chip). Ques...
| 2022-04-06 12:06 AM | ||
We are using Motion_AC to calibrate Accelerometer Offset & Scale, and Motion_GC to calibrate Gyro O...
| 2022-03-21 10:16 PM | ||
The current script in BlueSTSDK examples (https://github.com/STMicroelectronics/BlueSTSDK_Python) n...
| 2022-03-16 09:57 AM |