Subject | Author | Posted | |
---|---|---|---|
Hello everybody, I wanted to simulate the Sent_Protocol with a STM32 µC or simulate it as if I h...
| 2019-03-01 04:34 AM | ||
What is the package marking of LIS2DE12TR? Are there multiple versions of package markings? If so...
| 2019-02-28 10:57 AM | ||
Hello! Have bought the STEVAL-MKI183VI for the LIS2HH12 device. The device are enabled for al...
| 2019-02-26 09:19 AM | ||
I am using the STM32F407 discovery board and Wolfson pi audio interface. I have a problem in analys...
| 2019-02-26 07:55 AM | ||
Hi, I am following the guide "Getting started with the STMicroelectronics X-CUBE-BLE1 software ...
| 2019-02-25 07:50 AM | ||
Hi, I am using STM32F101VD to communicate via I2C with MPU6050 IMU device. Data transfer (readin...
| 2019-02-22 08:47 AM | ||
Discover how the AlgoBuilder platform streamlines algorithm development for STM32 microcontroller a...
| 2019-02-19 04:31 PM | ||
2019-02-18 01:44 AM | |||
Hi, I am following the guide "Getting started with the STMicroelectronics X-CUBE-MEMS1 software pac...
| 2019-02-13 03:10 AM | ||
LIS2DH12 is Configured with BDU=1, Normal Mode, FS=2G. While doing the below step after collecting ...
| 2019-02-11 11:43 AM | ||
CTRL_REG2=00; CTRL_REG3=00; CTRL_REG4=0x80;CTRL_REG1=0x47 with this BDU =1, FS=2G, Normal. ReadDat...
| 2019-02-11 11:05 AM | ||
Hi, We have a LIS2DW12 and a S2-LP setup on the same PCB, both using SPI. We have found that the...
| 2019-02-11 06:50 AM | ||
Hello, I'm planning on using the LSM6DSL in my design. For the same reason I have bought & work...
| 2019-02-11 04:19 AM | ||
hello, i am using stm32F401Re nucleo with stm mems sensor kit (x-nucleo-iks01a2). i am ...
| 2019-02-10 01:30 PM | ||
I am interfacing to an LSM6DS33 with an ST32F407using the SPI bus. The SPI is set up as follows: ...
| 2019-02-09 02:44 PM | ||
Here below the second part of the algorithm describing the basic PEDOMETER. The picture here below ...
| 2019-02-08 03:00 AM | ||
This example describes how to set up a finite state machine to enable the built-in detection of a b...
| 2019-02-06 08:37 AM | ||
The LIS3DSH datasheet contains the following text (not very clear): "If a receiver can’t receive a...
| 2019-02-06 12:32 AM | ||
Hi, is ST planning to release new version of the X-NUCLEO-IKS01A2 sensor expansion board with the n...
| 2019-02-05 06:40 AM | ||
Hello, I have configured LIS2DH12 to generate interrupt on INT2 pin on activity as well as a str...
| 2019-02-04 09:26 PM |