| Subject | Author | Posted | |
|---|---|---|---|
|
Hi everyone, I’m working on an STM32MP157F-EV1 board and encountering this error: warning: FBIOPU...
| 2025-03-14 9:44 PM | ||
|
Moved from MCUs section - STM32 is an MPU. Hi all, I'm developing a firmware for a custom board...
| 2025-03-11 8:37 AM | ||
|
Hello! everyone.
//-------------- Host -------------
OS: Ubuntu 22.04
Kernel: Linux leonsu-MI...
| 2025-03-05 12:22 AM | ||
|
Hello, I am struggling with improper color management for our display connected as LTDC. I prompt ...
| 2025-02-26 3:18 AM | ||
|
Dear all, we use custom board with STM32MP1 SoC onboard. We use Yocto with OE, STM, Qt and cus...
| 2025-02-25 1:36 AM | ||
|
Hello, I have a problem after cross-compiling retroarch from my PC to an STM32MP135 (ARM32), after ...
| 2025-02-13 2:29 AM | ||
|
Hello, I wonder if it is possible to put a game emulator on an stm32mp135-dk1 under openstlinux yoc...
| 2025-02-11 12:57 AM | ||
|
Hiii,
i am using STM32mp257f-ev1 , in this board i installed chromium and its working properly bu...
| 2025-02-10 11:13 PM | ||
|
Hi,ST professor. I am now using stm32mp135faf7 chip. I want to encrypt my TA application(optee_...
| 2025-02-06 6:53 PM | ||
|
On dev board STM32MP157f-dk2, I ran application in Qt, several gauges and measurements on DSI displ...
| 2025-02-06 9:45 AM | ||
|
Hi, I want to use the M4 core to handle all Audio DSP work I can see that MXCube allows the SAI po...
| 2025-01-28 7:33 PM | ||
|
Dear ST Team, The kernel recipe in Scarthgap branch has following packaging: FILES:${KERNEL_PACKA...
| 2025-01-19 10:41 AM | ||
|
Hi, On my STm32MP157c-dk2 with openstlinux-eglfs, I configured in device tree (*.dts file) CAN and...
| 2025-01-18 7:50 AM | ||
|
Hello, to retrieve the temperature in the M4 domain I use the documentation RM0436, page 1571 (des...
| 2025-01-16 2:36 AM | ||
|
Hi, I try to use libpq library to connect postgresql from STM32MP157. It works on my computer. Whe...
| 2025-01-13 11:53 PM | ||
|
Hi there, The commit in question is rather huge and the general complaint is that commit message s...
| 2025-01-06 5:09 AM | ||
|
I am trying to create virtual keyboard in STM32MP157D-DK1. But while making I am getting this error...
| 2024-12-27 1:00 AM | ||
|
Master: I've been learning stm32mp157 recently, and I've encountered some problems with less det...
| 2024-12-19 7:36 PM | ||
|
I'm pleased to share stm32mp-sign-tool with the community : It is a lightweight open-source alt...
| 2024-12-17 10:40 AM | ||
|
I have been using 1.16 workspace on cube IDE but today upon opening, the convert to C++ option was ...
| 2024-12-06 12:19 PM |