| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, I am testing TBB on a stm32mp157f-dk2 platform, yocto, kirkstone, sp_min version. I am wonderi...
| 2025-06-20 12:16 AM | ||
|
Dear sir/mam, We are currently working on generating interrupts for USB functionality. As pe...
| 2025-06-18 5:21 AM | ||
|
Hi there, I am in the process of creating a custom machine for the STM32MP257F-DK board following ...
| 2025-06-18 2:56 AM | ||
|
Hello, I'm trying compiling OpenSTLinux 6.6 for STM32MP257-EV1 using developer package + X-LINUX-R...
| 2025-06-16 8:27 AM | ||
|
I have a STM32MP135 with a M24C64 64k bit I2C EEPROM. The EEPROM is divided into NVMEM cells, which...
| 2025-06-15 8:22 AM | ||
|
Hi everyone, I’m struggling with an OpenAMP / RPMsg problem on an STM32MP157 (M4 core). When I co...
| 2025-06-08 1:25 PM | ||
|
Hi there, I followed the instructions as mentioned below. repo init -u https://github.com/STMic...
| 2025-06-03 6:35 AM | ||
|
Hi, i want to use the secure storage feature of our custom STM32MP151CAA based platform. Therefore...
| 2025-06-02 1:41 AM | ||
|
Hello We have custom board with STM32MP257DAI3 Processor.We would like to test it using Buildro...
| 2025-05-29 12:50 AM | ||
|
Hello, I want to use a virtual keyboard on STM32MP257 now. Due to the possibility of porting some ...
| 2025-05-27 5:03 AM | ||
|
Hello We are currently working on reading NOR Flash(MT25QL128) device ID through OSPI interface...
| 2025-05-27 1:56 AM | ||
|
Hi all, I'm currently looking to get Trusted Firmware-M (TF-M) running on the Cortex-M33 core of a...
| 2025-05-15 6:50 AM | ||
|
Hi, I have enabled iwdg2 in tf-a, uboot (PV="v2023.10-stm32mp-r1") , optee (version 4.0.0-stm32m...
| 2025-05-13 7:04 AM | ||
|
stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar-gz from ECO 6.0 and only enabling the US...
| 2025-05-07 9:56 PM | ||
|
Hi, I wanted to know if it's possible to read the raw mipi-dsi data dump from the Linux kernel i...
| 2025-05-06 8:18 AM | ||
|
Hello! I have succesfully run some test using the model zoo services repo. For classification and o...
| 2025-04-25 6:45 AM | ||
|
This info i have got through chatgpt is this true? ...
| 2025-04-15 2:46 AM | ||
|
WARNING Screenshot
Hi ST Community,
I’m working with the STM32MP135D-FK (Boyard) board an...
| 2025-04-10 10:34 PM | ||
|
Hello, I am trying to interface the STM32MP157 to a dual die NAND. I have found this previous p...
| 2025-03-25 4:56 PM | ||
|
Hello, I have a problem with UART reaction time under Linux. I need to detect frame break/error si...
| 2025-03-20 5:06 AM |