| Subject | Author | Posted | |
|---|---|---|---|
|
Hi All, I created dts and defconfig patches for u-boot but when I checked the nodes with dm tree...
| 2024-12-03 1:22 PM | ||
|
Hi, I am using my custom board based on stm32mp1, and I want it boot silently, including tf-a, op...
| 2024-12-01 7:23 PM | ||
|
Hello i have STM32MP157 board with A7 and M4 processors, i am trying to setup OpenAMP which works w...
| 2024-11-30 4:52 PM | ||
|
Hello everyone, I get an error when booting Linux + initramfs The versions of the main components...
| 2024-11-25 5:06 AM | ||
|
I'm playing DOOM on my STM32-Computer (STM32MP151). It's playable for a smal resolution (320x240). ...
| 2024-11-20 2:51 PM | ||
|
Being relatively new to Yocto, I struggle a bit with some issues. I intend to use ADC channels in ...
| 2024-11-11 12:38 AM | ||
|
Hi, I am unable to see the can0/can1 interface on my brand new STM32MP2 Eval board after re-flashi...
| 2024-11-10 11:34 PM | ||
|
Hi everyone, I'm currently working on a project to set up the X-STM32MP-GNSS1 GNSS module with my ...
| 2024-11-08 9:29 AM | ||
|
Development environment: buildroot st/2024.02.3 Hardware: STM32MP157DAB1 (The schematic diagram is...
| 2024-11-07 1:22 AM | ||
|
Hi Everyone, I have problem with custom carrier and dts. I am using MP135 SoM from PHYTEC and when...
| 2024-11-06 12:38 AM | ||
|
Hi ST Team, i am facing the issues for installing the browser form the last 15 days, i did not g...
| 2024-11-05 9:01 PM | ||
|
linux内核源码当中的SAI,两个子模块如何同时进行接收,一般正点的sda用于发送,SDB用于接收 Translated to English linux kernel source ...
| 2024-10-29 11:36 PM | ||
|
Hi, I'm getting an exception stack on bootup: [ 3.882380] ------------[ cut here ]------------ ...
| 2024-10-23 12:28 PM | ||
|
Dear ST community, i don't know if any one encountered this issue before, however when i try to i...
| 2024-10-22 6:33 AM | ||
|
Hi! I'm using the provided Kernel software from ST. The Kernel from STM32CubeIDE. I have compiled...
| 2024-10-22 12:08 AM | ||
|
I have configure so my login session is done automatically. So once my STM32-OS starting at my STM3...
| 2024-10-20 10:33 AM | ||
|
Hello, According to the doc, the Padding header extension adds the rest of the bytes in the header...
| 2024-10-16 1:43 AM | ||
|
Hi in my custom board (stm32mp157f) i removed the IC (STUSB1600). and i try to flash the images o...
| 2024-10-08 3:57 AM | ||
|
Hi! Just want to say that I have made a linux distro called STM32-OS that works with all of STM32M...
| 2024-10-06 9:21 AM | ||
|
Hi , I try to connect my Pendrive to USB Hub port, but it is not connecting, when ever i remove th...
| 2024-09-23 9:36 PM |