| Subject | Author | Posted | |
|---|---|---|---|
|
When enabling the HDMI output for displaying on the screen/TV, one must run the following command ...
| 2024-09-22 2:43 PM | ||
|
Hello, I am trying to see if I can enable the J1939 protocols on the stm32 mp158d-dk1 board. I ...
| 2024-09-22 8:56 AM | ||
|
This is my RAM usage when I run OpenSTLinux on my custom STM32MP151 board with 512 MB RAM. Is that...
| 2024-09-10 2:53 PM | ||
|
Hi, I am debugging the STM32MP257F-EV1 board with a debugger via JTAG/SWD. The kernel version i...
| 2024-09-09 8:15 PM | ||
|
Hello, I am using Yocto (Kirkstone) to develop linux for my embedded linux device, which is stm32m...
| 2024-09-06 6:33 AM | ||
|
hi i need to change the frequency and timing of DDR as well as where i need to modify that one and ...
| 2024-09-05 5:09 AM | ||
|
I am working with the STM32MP157F-DK2 Discovery kit, and I would like to know if it's possible to: ...
| 2024-09-05 4:20 AM | ||
|
Hello We are Working on a custom board with STM32MP157AAA3 processor.We are using Buildroo...
| 2024-08-30 10:14 PM | ||
|
Hi I am using the discovery kit (STM32MP157F-dk2), i check the manual and i did not get the Actua...
| 2024-08-30 6:00 AM | ||
|
Hi Every One i am facing the issue to find the pins of PWM in the (STM32mp157f-dk2 ), i configure...
| 2024-08-29 11:01 PM | ||
|
I tried to replace the uImage and .dtb file inside the starter package. First I copied over the ke...
| 2024-08-26 3:34 PM | ||
|
Hi Team, We are currently working on a UAV detection project and are in the process o...
| 2024-08-21 5:45 AM | ||
|
I don't have the knowledge to look at the LCD touch screen specifications to determine if it can be...
| 2024-08-20 8:48 PM | ||
|
The Linux version I am using is 6.1.28, and the chip is STM32MP157D. Currently, the USB-OTG chip us...
| 2024-08-16 2:17 AM | ||
|
@Erwan SZYMANSKI I have followed the instructions on "https://wiki.st.com/stm32mpu/index.php?tit...
| 2024-07-08 10:29 AM | ||
|
I have been working with the Secure boot and OPTEE integration in my Custom board. All the reposito...
| 2024-06-14 12:28 AM | ||
|
I am trying to update dunfell to kirkstone on stm32mp157f-dk2. I am observing below issue in system...
| 2024-05-22 9:37 PM |