| Subject | Author | Posted | |
|---|---|---|---|
|
hey currently i am working on stm32mp257dak3 on myir myc-ld257 board in which i want to access RCC...
| 2026-01-31 3:11 AM | ||
|
Hello, I am facing an issue with DFU mode on an STM32MP157C when Secure Boot is enabled (OTP locke...
| 2026-01-28 11:48 PM | ||
|
I'm working on a custom stm32mp133d board and Yocto (latest release), but something has me quite pu...
| 2026-01-28 12:02 PM | ||
|
I'm bringing up a very simple board that uses STM32MP135 with LAN8742A-CZ-TR Ethernet PHY as on the...
| 2026-01-21 1:23 PM | ||
|
I'm trying to use pwm for backlight control in stm32mp257f-ev1, the same changes shown in below pat...
| 2026-01-06 12:08 AM | ||
|
Hi We have a custom board using STM32MP257F and would like to program external NIOR flash using...
| 2026-01-05 4:43 AM | ||
|
Hi ST Team, I am working on custom MPU board based on STM32MP257F-EV1 reference design. For our d...
| 2025-12-26 6:27 AM | ||
|
Dear ST Team, We are working on enabling and running the Cortex-M33 core on the STM32MP257F-DK boa...
| 2025-12-15 9:56 PM | ||
|
Hi! I'm going to compile packages to bild a web browser that is optimal for the hardware of MP2. ...
| 2025-12-12 1:26 AM | ||
|
Hi, I'm trying to understand what the viable options are. my goal is to be on more recent versi...
| 2025-12-03 4:18 AM | ||
|
Hello engineers, I'm using the latest version of CubeMX and creating a project with STM32MP135FAFx,...
| 2025-11-20 5:09 PM | ||
|
Hi,
I’m working on a custom board based on the STM32MP157DAC. U-Boot splash is enabled, psplash i...
| 2025-11-12 11:41 PM | ||
|
Cannot boot an m33 TA app from the RFS on a STM32mp257f-DK board running latest OpenSTLinux starter...
| 2025-11-05 5:48 AM | ||
|
Hello, I'm currently testing the security features of OP-TEE and need to use the HUK function of SA...
| 2025-11-05 1:59 AM | ||
|
Hello, everyone! I am trying to program files generated by CubeMX(6.15.0) onto the STM32MP257F-...
| 2025-11-03 11:37 PM | ||
|
I'm trying to perform ADC using PA3 (adc1_in15) and PF11(adc1_in2) pins of stm32mp157c-ev1 board bu...
| 2025-10-31 10:45 AM | ||
|
Hello. I am using LVGL to open a USB camera and capture NV12 640*512 video at 30fps. I want to com...
| 2025-10-28 12:08 AM | ||
|
Hi, I’m planning to use OpenSTLinux for an upcoming project and would like to confirm whether it s...
| 2025-10-15 11:59 AM | ||
|
Hello, I am currently using the DDR Utility in STM32CubeProgrammer to tune the DDR4 on my STM32MP2...
| 2025-10-10 5:56 AM | ||
|
Hi I have a board based on a STM32MP135F. I can see that CLK signal of my sdcard (SDMMC1) very ...
| 2025-09-29 9:00 AM |