Subject | Author | Posted | |
---|---|---|---|
Hi, STemWin Version 5.42 and 5.44 have no more Keil and IAR libs as in 5.40 and earlier. Is there...
| 2019-03-10 7:44 AM | ||
We're in a project phase where were adding peripherals incrementally and using cube to configure th...
| 2019-03-07 1:01 PM | ||
Hello, I just had a look at the lcd module of the bsp for the stm32f746g disco board. It seems to ...
| 2019-03-07 12:47 AM | ||
I'm working with the STM32F769I-Disco board which uses DSI to drive its LCD display. I'm seeing ...
| 2019-03-05 3:18 AM | ||
I am trying to use DCMI on nucleo-144 ST32L4R5 for using OV5640 camera. I generated code for this u...
| 2019-03-01 2:04 AM | ||
2019-02-28 6:38 AM | |||
There seems to be a problem in the generated project with the OS_TimeMS GUI time not being updated...
| 2019-02-27 7:27 AM | ||
Hi, It's written here that STM32H750 has a JPEG hardware encoder / decoder for faster GUI operat...
| 2019-02-26 1:02 AM | ||
Hello everyone, @Nawres GHARBI I am Trying to Generate code for STM32f746 discovery board,...
| 2019-02-24 5:52 AM | ||
Looking through the video mode examples that use SDRAM, I see that in BSP_SDRAM_MspInit() a DMA cha...
| 2019-02-21 3:03 PM | ||
I have a few questions about DMA2D. I do not want to create separate topics for each question, s...
| 2019-02-21 5:05 AM | ||
When I want to execute a certain callback after a certain widget has been pressed, I use the functi...
| 2019-02-20 1:40 AM | ||
Hello, I would really appreciate if you could provide a small example demonstrating how one can us...
| 2019-02-19 2:48 AM | ||
stm32f429i discovery board is undergoing various tests. There are many Layer-related functions in ...
| 2019-02-17 8:35 PM | ||
I have purchased LVDS display from Mouser, Also I have purchased SN65DSI85Q1-EVM board (DSI to lvds...
| 2019-02-11 4:22 AM | ||
Hi everyone, I'm using OV5640 and it supports the JPEG format. The camera is set 640x480. I'm con...
| 2019-01-31 10:07 AM | ||
I used STM32Cube_FW_F7_V1.14.0 to create a project that will use the STemWin library for its touch-...
| 2019-01-31 8:29 AM | ||
How to erase all items from LISTBOX item?
| 2019-01-30 2:57 AM | ||
How to add item to swipe list when update comes form other event in software. Now I write somethin...
| 2019-01-25 5:41 AM | ||
I am working on porting STemWin VNC server to my board based on STM32F407VGT6. I am using 3.5inch ...
| 2019-01-14 9:40 PM |