Subject | Author | Posted | |
---|---|---|---|
Hello, I have 32L4R9IDISCOVERY board with round display. When I set clock configuration of MIPI DS...
| 2019-04-11 1:00 AM | ||
Porting the basic JPEG_DecodingUsingFs_DMA from Discovery to custom hardware and I'm failing with t...
| 2019-04-09 2:58 AM | ||
I'm trying to connect stm32f103c8t6 board with ILI9325 LCD display. I have created a driver for it ...
| 2019-04-09 2:48 AM | ||
Is stm32F207ZGTx support TouchGFX.
| 2019-04-03 11:36 PM | ||
Which image formats does TouchGFX support? Because if I reduce the size of a PNG image, it loses qu...
| 2019-04-03 2:21 AM | ||
I have start to interfacing a TFT module which have RA8875L3N driver .Please share its library (API...
| 2019-04-03 12:49 AM | ||
I am using the STemWin BASIC_HellowWorld Application. I modified the source code to look like th...
| 2019-03-31 6:12 PM | ||
Kindly share me the library (preferably written with cubeMx32 APIs) written for Graphic LCD ST7920 ...
| 2019-03-31 5:49 AM | ||
Dear Members, I tried to print string on ST7735 ST7735_WriteString(0, 0, "Font_7x10, red on bla...
| 2019-03-28 10:21 PM | ||
I downloaded the IAR IDE and installed it, selecting the time-limited license so there isn't a limi...
| 2019-03-28 8:58 PM | ||
Hi Team, Am working with STM32L4F9 Discovery board Generated code for sample UI with emWin and a...
| 2019-03-25 10:13 PM | ||
Hello, I want to display the current time in TouchGFX project. I am using TGFX 4.9.3 (using Kei...
| 2019-03-25 4:25 AM | ||
I'm working on a custom board, where I'm introducing new features and testing each individually. ...
| 2019-03-22 9:37 PM | ||
Hi everyone, i enable touchgfx in my project starting with cubeMX. But it doen't run touchgfx. I...
| 2019-03-22 6:57 AM | ||
2019-03-22 10:44:08,257 [1] INFO TouchGFXDesigner.App: Logging configured 2019-03-22 10:44:08,270 ...
| 2019-03-21 8:06 PM | ||
Hello, To avoid context switches between the painting thead and DMA2D_IRQHandler interrupt I swi...
| 2019-03-18 11:51 PM | ||
Hello Community, I am working with a custom PCB powered by an STM32F769 that has Ethernet and LC...
| 2019-03-18 3:47 PM | ||
I want to use MC240064GD6W-FPTLW screen with my STM32F4 Discovery but it doesn't work. Can someone ...
| 2019-03-18 5:24 AM | ||
2019-03-16 4:45 PM | |||
I saw the datasheet of STM32F769xx and find two Version of LQFP176 with and witout DSI. I can find ...
| 2019-03-14 8:07 AM |