Subject | Author | Posted | |
---|---|---|---|
When using scroll wheel with text area, the controller falls into a hard fault, when I use the func...
| 2021-04-16 09:24 PM | ||
HI i try in callback repeat one memory line in two display lines, but display still show no double...
| 2021-04-15 01:47 AM | ||
Using version : IDE 1.6.1 GFX Designer: 1.6.1 MX : 6.2.1 Board : STM32L4R9 DISCORVERY First ...
| 2021-04-13 05:40 PM | ||
Hi guys, I would like to know, if I can somehow in general define img in program and use it in f...
| 2021-04-13 06:01 AM | ||
Hi @Martin KJELDSEN Please update gcc version bundlen with TouchGFX Environment to a newer ver...
| 2021-04-12 01:06 AM | ||
Hi all, How is it possible to change a particular index of Histogram graph? I would like to chang...
| 2021-04-11 09:41 AM | ||
Hello! I have a problem with my Swipe container. It is composed of three screens, and it works fin...
| 2021-04-06 11:51 AM | ||
Hi, In my Project i have a Texture Mapper to rotate an image(Z axis) with respect to vertical dr...
| 2021-04-06 05:03 AM | ||
Hello! I try to make powersaving mode for my device. So i should power off all chips on my board. I...
| 2021-04-06 03:46 AM | ||
My application demo is very simpe. I'm started with Cube MX 6.2.0 and the last stm32H7 Hal library...
| 2021-04-05 02:17 PM | ||
Hi all, is it possible to enlarge the ScrollBar by code?
| 2021-03-30 12:23 PM | ||
bmp data from "Bitmap(bmpid).getData()"
| 2021-03-29 03:22 AM | ||
Hi In GFX, I generate a template. In the IDE, I import a template. I don't have * .hpp in it. They...
| 2021-03-29 01:56 AM | ||
Hello, I am currently trying to control a TFT display (240x240 pixels) with SPI. I have followed ...
| 2021-03-26 02:51 AM | ||
I know i can use cc936.c of FATFS, but I think this is not a good method, because it will take up m...
| 2021-03-25 08:33 PM | ||
I've setup and built quite a bit of a project for a STM32F7508-DK through TouchGFX and STM32CubeIDE...
| 2021-03-25 06:09 AM | ||
2021-03-24 06:10 PM | |||
I use CubeMX to construct a project for RGB LCD in a STM32F767 custom board. MPU is enable, and is...
| 2021-03-23 09:02 PM | ||
Don't you think it's wrong to make canvasBuffer as member of StartupScreenViewBase class? As far a...
| 2021-03-23 01:08 AM | ||
2021-03-22 07:26 PM |