Subject | Author | Posted | |
---|---|---|---|
I integrated succesfully the feature binary translations so that i can load my texts from external...
| 2021-03-18 07:53 AM | ||
Once upon a time I did a project for displaying images from a camera OV5640 and STM32H743XIH6 Th...
| 2021-03-17 07:50 AM | ||
Hello, I am trying to port TouchGFX Designer generated code into an STM32 Project that is built in ...
| 2021-03-16 05:00 PM | ||
I'm trying to access the View's members including the protected ones from outside. I don't want to ...
| 2021-03-15 04:09 AM | ||
Hi all, i would like to know if in STM32CubeIDE exist a mode to show the ASCII value of a "touchgf...
| 2021-03-14 04:05 AM | ||
Hello , I am using STM32F429I-Discovery board I want to draw sprites on TFT-LCD with transparency ...
| 2021-03-13 02:37 PM | ||
Hello, I am trying to reconfigure my STM32H735G-DK to use HSI instead of HSE for a TouchGFX base...
| 2021-03-11 03:56 PM | ||
Hi, I use STM32CubeIDE and TouchGFX. Sending to "stm32f746 discovery board" using com port text. ...
| 2021-03-10 01:06 PM | ||
Hi, I am using STM32F407, trying to interface LCD 16x2 to display sensor data on it. using same c...
| 2021-03-07 12:12 AM | ||
Hi, I have a project for STM32L4R9AI and I have analog and digital clock screens. When I set con...
| 2021-03-02 09:35 AM | ||
Hi I'm gonna change size of a box progress .but it seems that it's size has just some predefined s...
| 2021-03-02 12:58 AM | ||
I am looking into using an STM32 with TouchGFX to drive a 4.3" TFT-LCD. The TFT-LCD will have ST728...
| 2021-02-25 12:26 AM | ||
I am using an STM32H7A3ZI and am seeing some unexpected behavior with the LTDC color keying in L8 m...
| 2021-02-24 03:53 PM | ||
Has anybody else used these library functions and found them to be incredibly slow? Just want to m...
| 2021-02-23 12:03 AM | ||
Hi all, I am doing one project where TouchGFX data has to be store in External Flash. For thi...
| 2021-02-17 05:05 AM | ||
Hello I'm just a beginner at STM32. I'm going to use 800 x 480 TFT LCD this time. First, I set LT...
| 2021-02-15 11:58 PM | ||
I have found a number of soulutions for this, but they all seems to be "old" and the make file that...
| 2021-02-11 02:41 AM | ||
Question 1: We are developing a custom board based on STM32H750B-DK. We have a “custom touch�? on...
| 2021-02-10 01:31 AM | ||
Hi! I am using STM32L496 on Nucleo 144 board CubeMX 6.1.1 CubeIDE 1.5.1 TouchGFX 4.16.0. After ge...
| 2021-02-07 04:52 AM | ||
We are going to test it by changing the LCD on the stm32f469i_Discoveryboard. The 5-inch LCD has...
| 2021-02-02 04:19 PM |