Subject | Author | Posted | |
---|---|---|---|
Hello, We have successfully been using this LCD module with TouchGfX. On a unit we have left ru...
| 2021-08-12 08:49 AM | ||
Hi, I want to check if there is a message sent from the backend task in every tick event. I am usi...
| 2021-08-11 07:29 AM | ||
After connecting STM32 to LCD, there is no response when I tap on the screen; after connecting Ardu...
| 2021-08-11 12:41 AM | ||
I'm working with touchgfx using C++ in Visual Studio 19 and I'm trying to configure the simulator e...
| 2021-08-10 08:04 PM | ||
I've read the Release Notes and they say nothing about any bugs that may have been fixed going from...
| 2021-08-10 05:24 PM | ||
2021-08-08 03:05 AM | |||
Hi I had a probelm when I ported the program I use FSMC(8080) ,and I reffered to the stm32f412-di...
| 2021-08-07 01:41 AM | ||
Hi, In the TouchGFX license it states that: "No use, reproduction or redistribution of this s...
| 2021-08-06 09:46 PM | ||
I setup a scroll list with particular template with n items. Since the items currently fit to the s...
| 2021-08-04 04:03 PM | ||
I have a lot of custom containers to define. When I want to scroll down the list to see ones on bot...
| 2021-08-04 05:13 AM | ||
MX congiuration: FreeRTOS task: XHAL: result: because my custom board not have t...
| 2021-08-04 12:57 AM | ||
Could anyone suggest how to do... I have application with multiple screen, should be 200 or more. ...
| 2021-08-03 10:26 PM | ||
I setup a radio button using my own image instead of one provided by TouchGFFX Designer. Initial si...
| 2021-08-03 06:15 PM | ||
2021-08-03 06:39 AM | |||
Hello, I want to rotate 90 degrees to display the debug strings, but I can't find a function f...
| 2021-08-02 05:34 PM | ||
Hi, I'm using an STM32H725 with TouchGFX. I using a custom FMC interface to an LCD. I'm using the ...
| 2021-07-30 01:38 PM | ||
Hello, I'm having a new problem with a touchGFX designer, when i try to add a new screen the CUBE I...
| 2021-07-30 07:33 AM | ||
Hello everyone, I have a Mikromedia 7 Capacitive board, which includes a STM32F746ZG, a LCD Disp...
| 2021-07-30 05:44 AM | ||
So assume I define a swipe container which has two pages. When I swipe to leave page0 to page 1, I ...
| 2021-07-28 09:42 PM | ||
Assume we setup a swipe container which contains multiple pages. One of the pages is scroll list wh...
| 2021-07-28 09:39 PM |