Subject | Author | Posted | |
---|---|---|---|
Hello Community, I am trying to integrate a deep neural network into the micro-controller with t...
| 2022-07-18 7:47 AM | ||
Hello, I created my model using Colab and saved it as .tflite (tensorflow version is 2.8.2) I wan...
| 2022-06-30 7:37 AM | ||
Hello, the question may be stupid but everywhere I go I see people using the STM32H747 for the diff...
| 2022-06-10 4:46 AM | ||
Hi, it seems to be a common error in STM32 devices. It happens when I try to validate on target aft...
| 2022-05-27 1:40 PM | ||
I have a model file(.h5) and Analyze is failing with keras(.h5) model at STMCubeMX and throwing INT...
| 2022-05-20 1:28 AM | ||
E200(ValidationError): stm32: Unable to bind the STM AI runtime with "network" c-model: [] con...
| 2022-05-09 11:30 AM | ||
We have created an LSTM model using Keras, and decreased its size to use it on our STM32F746G-Disco...
| 2022-05-05 3:09 PM | ||
I am looking for a development board that can run a deep learning model with a CSI interfaced CMOS ...
| 2022-03-28 7:50 PM | ||
I am trying out a code example from Nano Edge AI studio and want to download and run that on the S...
| 2022-03-11 10:51 AM | ||
I want to try and get more information about x-cube-ai. I have prepared the neural network and I ...
| 2022-03-08 1:40 PM | ||
About the function "validate on target", I don't understand what X-cross is. And when I clicked th...
| 2022-03-03 8:30 AM | ||
Hi, I am using Stm32cubeide for creating a tinyml project for sinewave-tensorflow example. For thi...
| 2022-01-10 8:04 PM | ||
I am using the STM32L476RG with its respective NUCLEO board. I want to experiment with object detec...
| 2022-01-06 4:20 PM | ||
I am importing a tf lite model using tf lite runtime library in XcubeAI 7.0. I also tried with XCub...
| 2021-12-14 4:39 AM | ||
I'm trying to create an AI Vision application based on the STM32H747I_DISCO_FoodReco_Quantized appl...
| 2021-12-07 5:29 AM | ||
Hi everyone, I developed and trained a simple neural network in MatLab. I exported it as an ONNX fi...
| 2021-11-29 1:11 AM | ||
Hi. I currently try to do FP-AI_Vision Person Detection . so I would like to be setting STM32H747i...
| 2021-11-23 1:31 AM | ||
In the recent workshop for "Enabling Intelligence at the Edge with STWIN and NanoEdge AI Studio", ...
| 2021-11-22 6:37 AM | ||
2021-11-12 3:42 AM | |||
2021-11-08 11:16 PM |