Subject | Author | Posted | |
---|---|---|---|
When I'm trying to analyze the network in CubeMX I get the following error: TOOL ERROR: Unsuportet...
| 2020-03-24 2:24 AM | ||
Hello, I created a CNN model used Keras with tensorflow here's the model model = models.Sequ...
| 2020-03-17 5:52 AM | ||
Hello, I am using STM32CubeMX Ver 5.5.0 with X-CUBE-AI . In the generated code inside function ...
| 2020-02-26 2:22 AM | ||
I recently found out about the STM32Cube AI toolkit, which holds much promises. In the ST blog they...
| 2020-02-24 1:28 AM | ||
aiSystemPerformance.c : line 937 and 940 for (int i = 0; i < net_exec_ctx[idx].report.n_inputs; i...
| 2020-01-10 8:33 PM | ||
This is the log of Validation on Desktop Starting AI validation on desktop with random data... ...
| 2019-11-07 8:12 AM | ||
Hi experts! I am trying to use a NN made on Keras on my NUCLEO-F303K8 (MCU STM32F303K8T6). I've...
| 2019-10-03 7:36 AM | ||
Hi, I'm planning on implementing a motor fault detection through vibration signals on an embedded ...
| 2019-09-17 6:54 PM | ||
I have two different input data (voltage, current) and output data in excel file. I need help to tr...
| 2019-09-09 11:13 PM | ||
2019-09-01 3:09 AM | |||
2019-09-01 2:16 AM | |||
2019-08-22 7:27 PM | |||
Hello, I used the Pruning API of Tensorflow and reduced the weights of my model. If i import the...
| 2019-08-22 7:37 AM | ||
I am trying to validate Keras model using STM32 cubeMX on STM32f407 discovery kit. I am able to g...
| 2019-08-08 2:58 AM | ||
I am trying to use X-cube-ai in STM32CUBEIDE but when I try to configure I am getting this error " ...
| 2019-08-07 1:04 AM | ||
Hello, On ST youtube channel there's a demo for character recognition, image classification https...
| 2019-07-09 7:45 AM | ||
I have made a model for imdb dataset in keras that looks like: model = Sequential()
model.add(Emb...
| 2019-04-28 12:10 PM | ||
Hello, I am using CubeMX 5.1.0 with the X-CUBE-AI 3.4 package. It works really fine with Atollic...
| 2019-04-25 5:17 AM | ||
Hi, I made a small Python script that allows to convert models from the commandline. Wraps the sam...
| 2019-04-01 6:29 AM | ||
Hello!! When I was learning the CubeMX.AI I could not find additional software's contains in my wi...
| 2019-02-14 6:31 PM |