Subject | Author | Posted | |
---|---|---|---|
Could you send me the .ioc for the STEVAL-STLCR01V1. If it is not possible how I have to do the cub...
| 2022-12-16 10:36 AM | ||
2022-12-12 2:58 PM | |||
I'm using X-CUBE-AI version 7.3. I'm trying to generate code for my .tflite model using STM32Cube.A...
| 2022-12-12 11:01 AM | ||
https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8 Lab03, I wasn't able to...
| 2022-12-06 9:09 AM | ||
Hi! I am doing some experiements to analyze the neural network model. The model I am using is the H...
| 2022-11-26 11:02 AM | ||
Hi, for now, the evaluation is accuracy, rmse, mae, l2r. But I'd like to evaluate my model by F1 sc...
| 2022-10-31 4:17 PM | ||
I am trying to flash USB_webcam example from FP-AI-VISION1 pack on my stm32h747i-disco board by pas...
| 2022-10-30 8:34 AM | ||
There are several threads concerning FFT's on a ST Micro based ARM processor. We're developing CNN ...
| 2022-10-22 5:37 PM | ||
Kindly help us rectify this error in network.c file
| 2022-10-21 2:27 AM | ||
I have created a project which uses the Nucleo-H7A3ZI-Q. When I build the project is completed succ...
| 2022-10-16 2:25 PM | ||
Starting AI validation on target with random data... C:/Users/Ashu/STM32Cube/Repository/Packs/S...
| 2022-10-12 11:51 PM | ||
Hi,the code is successfully generated and built on cubeide,download to the board and it passed the ...
| 2022-10-12 8:39 PM | ||
Hello, I seem to not be able to run model analysis on CubeAI. I use a Mac mini with M1 Apple Silic...
| 2022-10-03 11:55 AM | ||
I'm using the STM32 IDE, making a project for my Nucleo-G474RE. I've loaded the X-Cube AI software ...
| 2022-09-28 9:55 AM | ||
Hello, everyone. I had a problem with version 7.2.0 of X-CUBE-AI. I load a keras 1D-CNN mode...
| 2022-09-22 7:46 PM | ||
2022-09-18 6:37 PM | |||
Hi all, I tried to porting AI model which I made with cubeAI but it seems like not work. I ...
| 2022-08-30 12:49 AM | ||
I realize you can use the stm32ai tool to find the SRAM/Flash usage of the model. However, this doe...
| 2022-08-16 3:27 PM | ||
Hi friends, I am now trying to bring .h5 model to my board. So just following tutorial from st....
| 2022-08-08 4:02 AM | ||
Hello. I evaluate the SensorTile Kit with the following combinations. Core system STLCS01V1 Cra...
| 2022-08-03 8:43 PM |