Subject | Author | Posted | |
---|---|---|---|
I use x-cube-ai 6.0 version & stm32h747i-disco board. By clicking on the [Advanced Settings] butto...
| 2021-03-30 12:00 AM | ||
Hello dear Engineers, I have a system with 3 inputs and 3 outputs. The system outputs are complete...
| 2021-03-24 1:28 AM | ||
Hello, I have a STM32F746G-DISCO which has a microcontroller with 1 Mbytes of Flash memory and 340 ...
| 2021-03-23 7:43 PM | ||
Hi, I am working for a ‘Digit detection’ project using STM32CubeIDE 1.5.1 (X-CUBE-AI.5.20) and STM...
| 2021-03-07 4:48 AM | ||
In the project, the input data of keras model is a 2-d vector consisted of float x1 and float x2. B...
| 2021-02-02 9:47 PM | ||
Hi all, I am trying to build a tensorflow model on STM32G474RE chip, I've got my model.tflite and...
| 2020-12-23 2:07 AM | ||
Hi, I am using stm32l476, i am trying to run an AI validation project. i replaced the UART wi...
| 2020-11-04 4:18 AM | ||
Hi, I am using STM32F769I-DISCO. I want to make a system that can recognize different sounds with ...
| 2020-10-08 7:39 PM | ||
the model I have bulit: the config of my project: only use cubemx.ai for Application Template,...
| 2020-09-24 10:14 PM | ||
Here i only found years old https://community.st.com/s/question/0D50X00009XkZkuSAF I have idea i...
| 2020-09-15 10:08 AM | ||
Hello, I am currently using X-CUBE-AI library to run neural networks on a stm32h747. I successfu...
| 2020-08-11 3:04 AM | ||
2020-07-30 2:36 AM | |||
I am using the STM32H745ZI-Q Dual Core MCU. My workflow is to generate the AI library using a Sin...
| 2020-06-18 5:33 AM | ||
Hello, I am under graduate student in Korea and I have a question to solve a little of problem....
| 2020-06-03 4:51 AM | ||
2020-05-17 6:11 AM | |||
Hello everyone, I would like to ask you about a handwritten number recognition project I have been ...
| 2020-05-12 8:18 AM | ||
I have OV7670 camera and Nucleo-L496ZG development board, Is it possible to run AI model using them...
| 2020-05-04 11:44 PM | ||
Hello, I successfully used a post-training quantized TFLite Model in X-CUBE-AI. Nonetheless, I c...
| 2020-05-04 9:24 AM | ||
Hi all, I recently got a STM32H747 DISCO kit, however, this is my first time using stm MCUs, and...
| 2020-04-24 3:47 PM | ||
2020-04-11 11:27 PM |