Subject | Author | Posted | |
---|---|---|---|
When i want to init uart8 static void MX_USART8_UART_Init1(void) { huart8.Instance = UART8; hua...
| 2023-08-08 5:25 AM | ||
I am using NUCLEO-L4R5ZI MCU to communicate with Murata SCA3300 sensor. As an initial step I am try...
| 2023-08-08 2:17 AM | ||
Is this possible to update firmware from an STM32 device to NRF device over ble. Need step-by-step ...
| 2023-08-08 1:24 AM | ||
i use STM32F439ZIT6U
and activate crypt function like below capture
and use library fu...
| 2023-08-08 12:44 AM | ||
In one of my projects I'm using USB Host with STM32F407, It's working fine for both keyboard and mo...
| 2023-08-07 11:58 PM | ||
Can't find a source file at "C:/Users/mmm/Documents/Projects/stm32 projects/AccessMini/Debug/../Cor...
| 2023-08-07 6:14 AM | ||
Hi, We are working on a project based on the x-cube-aws package. I used the script from the GitHub...
| 2023-08-05 7:16 PM | ||
Hello, Recently I started looking at the STM32F7 to implement a high quality audio front end (AFE)...
| 2023-08-04 11:20 AM | ||
please let me know my coding is correct ,whether usage of my exti is correct while (1)
{
H...
| 2023-08-03 8:50 AM | ||
I was trying to interface a microSD card (32GB) with STM32F407 through SDIO. Tried 1-bit and 4-bit ...
| 2023-08-03 1:03 AM | ||
Hello There, I'm already using LTDC peripheral for the display interface and aware of LTDC sync pa...
| 2023-08-02 5:54 AM | ||
this part in my code completely making my prototype to sleep which should not.As my standby should ...
| 2023-08-02 3:03 AM | ||
i was trying to work on bluepill stm32f103c6t6 i triedto send can msgs in loopback mode but im not ...
| 2023-07-27 10:40 PM | ||
Hello, I initialized CAN on STM32F429ZIT6 on registers. I would like to tranmitt and receive messag...
| 2023-07-26 3:36 AM | ||
Normal mode of FDCAN is not working. Attached project file here. Please suggest if any changes are ...
| 2023-07-25 11:33 PM | ||
I am using a P-NUCLEO-LRWAN3 product. 1- At the beginning, I need to change ETHERNET: DHCP to STA...
| 2023-07-25 11:13 PM |